Premier Farnell is now shipping the Infineon EasyPIM™ IGBT7 Modules with TRENCHSTOP™ technology: The Right Fit for Industrial Drives
New Easy module offers straight-forward, time-to-market design whilst bringing system cost savings to industrial drives
![Inline_green Inline_green](https://content.presspage.com/uploads/1564/1920_inline-green-748754.jpg?10000)
Premier Farnell, the Development Distributor, is now shipping the new 1200 V TRENCHSTOP™ IGBT7 and emitter-controlled EC7 diode from Infineon. Packaged in the well-known Easy housing, this EasyPIMTM IGBT7 provides higher power density, lower system cost, and reduced system size. The 1200 V TRENCHSTOP™ IGBT7 and EC7 diode technology is based on latest micro-pattern trenches technology and optimized for industrial drive applications which means much lower static losses to meet energy efficiency requirements, softer switching and improved controllability. Additionally, by raising the allowed maximum overload junction temperature up to 175 °C in the power module, a significant increase of power density can be obtained.
The 1200 V TRENCHSTOP™ IGBT7 is available in a range of modules; the EasyPIM™ 1B 1200 V, three phase input rectifier PIM (Power Integrated Modules) in 10 A and 25 A options and the 1200 V sixpack IGBT module EasyPACK™ 2B 1200 V, 100 A sixpack IGBT module. The new modules are designed with the same pin out as TRENCHSTOP IGBT4 modules, which support design engineers in reducing design effort. New modules also enable a higher output current in the same package, or the similar output current in a smaller package resulting in more compact inverter designs where needed. All module types are equipped with Infineon’s reliable PressFit mounting technology for low ohmic resistance and reduced process time.
Key benefits of TRENCHSTOP™ IGBT7 include:
-
Low losses - new chip technology shows extremely lower losses with optimized low Vce(sat).
-
dv/dt optimized for 2-8kV/µs, tailored for drive application.
-
Short circuit is tailored for better performance, 8µs @150°C is enough for drive application.
-
The gate drive is simpler and optimised for application condition. Only a gate resistor is enough to control.
-
Increase of Tvjop up to 175°C increase the power density.
-
Best-in-class VCE(sat).
-
Operation at 175°C at overload.
-
Enhanced controllability optimized for drive applications.
-
Higher power density - Same power in 35% smaller package.
The Infineon 1200 V TRENCHSTOP™ IGBT7 and emitter-controlled EC7 diode modules are available from Farnell in EMEA, Newark in North America and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/