Premier Farnell introduces the TGF4000 Series from Aim-TTi providing class leading performance alongside unrivalled value for money
Series offers true dual channel, high-performance programmable function/arbitrary generators from 40MHz up to 240MHz
Premier Farnell has added the TGF4000 series function/arbitrary generator from Aim-TTi to its linecard for same day despatch. This latest launch from Aim TTi utilises 20 years of experience in the industry to address demand from customers for increasingly high frequency and precision in their test signals. The TGF 4000 series delivers high precision, wide bandwidth models with class-leading performance alongside unrivalled value for money. At the higher end of the series, the new TGF4162 and TGF4242 offer extended frequency and level that may not have been affordable to customers previously.
The TGF4000 offers key advantages over other models in this price range as a true dual channel generator. The series has two full capability channels which can be operated completely independently as if they were two separate generators, or in coupled or tracking modes with precise channel to channel phase control at a resolution of 0.0010.
The TGF4000 series also out-performs other generators in its price range by offering models at up to 240MHz with low harmonic distortion and phase noise. In addition to a wide selection of modulation types from either internal or external signal sources, the TGF has a built-in wideband noise generator that is useful for customers evaluating design performance degradation with defined levels of signal noise. Audio band THD is significantly better than similar generators at just 0.05% and Pulse jitter is dramatically lower than any comparable generator at only 30ps.
Key features include:
- 0.001mHz to 240MHz (TGF4242), 160MHz (TGF4162) , 80MHz (TGF4082) or 40MHz (TGF4042) sine frequency range
- High sine wave purity with low phase noise and jitter, audio band THD down to 0.05%
- Arbitrary waveforms of 14-bits / 400MSa/s (TGF4042 & TGF4082) or 16-bits / 800MSa/s (TGF4162 & TGF4242)
- Comprehensive internal/external digital and analog modulation set including Sum* modulation
- Harmonics generation using up to 16 harmonics*
- Two identical channels - independent or linked with coupled and tracking modes
- 1mHz to up to 100MHz Pulse generation with 100ps width resolution, <30ps jitter and independently variable rise/fall times.
- PRBS pseudo-random bit sequence generation with 8 sequence lengths*
- 125MHz frequency counter/timer with five measurement modes
- Wideband noise generator with up to 100MHz noise bandwidth
In addition to these features, the TGF4000 series is equipped with a 4.3 inch high resolution colour screen, providing added efficiency and clarity when carrying out complex testing. Graphs for both channels can be displayed side by side for easy comparison or alongside a detailed description of the settings selected, with each channel displayed in a set colour to provide instant recognition of the output channel when altering and updating settings or preferences.
The TGF 4000 series is available from Farnell element14 in EMEA, Newark element14 in North America and Mexico and element14 in Asia Pacific.
Features marked * are only available on the TGF4162 & TGF4242
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com