London,
25
September
2018
|
01:00
Europe/Amsterdam

Premier Farnell helps customers take control of their environments with the addition of Purrmetrix data logging sensors and gateways

Flexible sensors and gateways suitable for facilities management, energy management and more

purrmetix feature

Premier Farnell has added Purrmetrix to its line card for data logging sensors. Purrmetrix brings an entirely new approach to data loggers. Unlike existing data logging products it needs no one to collect or download data from the sensors and the data is transmitted live to the Purrmetrix web service.

The range of data logging sensors and sensor gateways allow users to measure log and analyse a range of environmental variables including temperature, humidity, CO2 and occupancy, making it possible to quickly build a deep understanding of the conditions affecting anything from a greenhouse to a housing estate. The flexible and low-cost sensors and gateways are suitable for a broad range of industries including facilities management, energy management, Data Centres, social housing and agriculture.

Purrmetrix allows up to 200 small, lightweight sensors to connect wirelessly to the Purrmetrix gateway which sends data in real-time to the Purrmetrix servers. The system is flexible, allowing users to position sensors exactly where they are needed, and quick and easy to set up, enabling users to get from opening a box of sensors to getting information within half an hour. A comprehensive array of analytical templates, including heat maps and waterfalls, allow users to see the information graphically, in real-time or to replay conditions over any timescale chosen. The low power sensors have a battery life of approximately 3 years.

As data is delivered in real time it can be used for constant (and consistent) monitoring, reporting, recording, analysis and action. Data can also be linked to email alerts or exported from the system via an API to other cloud based services like BMS, CAFM, task managers or any other IoT platform.

Key benefits of the Purrmetrix system include:

  • Extremely rapid to install and configure
  • Wireless, allowing sensors to be located exactly where they are needed
  • environmental data accurately positioned into plan or model of buildings
  • alerts and analysis available on many types of live environmental data
  • API integrates analysis into task management software or building service controls
  • Competitive cost vs data logger products

Simon Meadmore, Global Head of Semiconductors for Premier Farnell and Farnell element14 said: “The cost advantages and ease of installation of Purrmetrix data logging system, means multiple data points can be used to give enhanced information for decision making, quickly and without previous experience. Purrmetrix will change the way environmental data is collected, viewed and used – putting the power of accurate data directly in the hands of the end user.”

Purrmetrix range of sensors and gateways is available from Farnell element14 in Europe, Newark element14 in North America and element14 in APAC.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com