Pre-order the Latest Raspberry Pi 5 boards from element14
The faster and more powerful Raspberry Pi 5, featuring improved CPU and GPU performance, camera, display, and USB interfacing is available to order on September 29th
![Raspberry Inline.jpg Raspberry Inline.jpg](https://content.presspage.com/uploads/1564/5078db4b-db38-45ee-bd93-adc9c696425f/1920_raspberryinline.jpg.png?10000)
The much-anticipated new Raspberry Pi 5 4GB and 8GB boards will be available for pre-order from element14, Raspberry Pi’s exclusive global licensee, on 29th September.
Raspberry Pi 5 delivers a two-to-three times increase in performance over Raspberry Pi 4, including a significant boost to GPU performance, together with improvements to camera, display, and USB interfacing. These interfacing improvements are delivered by the RP1 I/O controller chip, designed in-house at Raspberry Pi, and marking the first time Raspberry Pi’s proprietary silicon has featured on a flagship product.
Key features of the new Raspberry Pi 5 include:
- 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, with 512KB L2 caches and a 2MB shared L3 cache.
- VideoCore VII GPU.
- LPDDR4X-4267 SDRAM.
- 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi.
- Bluetooth 5.0 / Bluetooth Low Energy (BLE).
- Micro SD card slot, with support for high-speed SDR104 mode.
- 2 × USB 3.0 ports, supporting simultaneous 5Gbps operation and 2 × USB 2.0 ports.
- Gigabit Ethernet, with PoE+ support (requires PoE+ HAT).
- 2 × 4 lane MIPI camera/display transceivers.
- PCIe 2.0 x1 interface for fast peripherals.
- 5V/5A DC power (PD enabled).
- Raspberry Pi standard 40-pin header.
- Real-Time Clock (RTC), powered from external battery.
- On-board power button.
Other enhancements available for users include a new case with improved thermal features, featuring an integrated variable-speed fan, powered and controlled from a dedicated connector on the Raspberry Pi 5 PCB. An active cooler provides an alternative cooling solution for customers who wish to use their Raspberry Pi 5 under sustained heavy load without a case; and a new 27W USB-C PD (Power Delivery) Power Supply delivers a maximum of 5.1V, 5A enabling the Raspberry Pi 5 to power a wider range of peripherals.
Eben Upton, CEO at Raspberry Pi said: “Raspberry Pi 5 is the single largest engineering program we’ve ever undertaken, spanning more than half a decade. We’re hugely excited by the performance of the completed product: a no-compromises Linux desktop computer from just $60. element14 has been a Raspberry Pi licensee since the launch of the original product in February 2012, and are now our sole licensee: we are delighted to be working with them to bring our latest and most powerful flagship product to a global audience.”
Simon Meadmore, VP Product and Supplier Management at element14 said: “element14 is proud to be the exclusive global manufacturing licensee for Raspberry Pi 5, building on the phenomenal success of Raspberry Pi 4. The new boards offer users an impressive increase in CPU and GPU performance, together with many improvements to camera, display, and USB interfacing that together will provide exciting new opportunities for enthusiasts around the world.”
Pre-orders placed with element14 from 29th September will see shipping commence in late October from Farnell in EMEA, and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/