Keysight Infiniium S-Series Oscilloscopes Now Available from Newark
New range offers the industry’s best signal integrity to meet pressing measurement challenges
![FAR507_inline FAR507_inline](https://content.presspage.com/uploads/1564/1920_far507-inline-407454.jpg?10000)
Newark, the Development Distributor, today announced a new line of Keysight Technologies oscilloscopes, adding to its extensive range available for same day shipping. With the industry’s best signal integrity, Infiniium S-Series oscilloscopes offer the most advanced platform for designers and engineers to see the truest representation of their signal.
For designers debugging their latest design or verifying compliance, it’s critical that the oscilloscope displays accurate signal measurements. This requires world-class signal integrity, and the Infiniium S-Series oscilloscopes are designed with that in mind. The S-Series provides a superior time base, front-end, and ADC technology blocks, giving designers and engineers a platform with up to 16 bits of resolution, low noise, low jitter, and high ENOB. These benefits give users visibility into the true performance of devices, ensuring safe and confident measurement.
The S-Series can be applied to difficult-to-probe signals, small voltage signals tough to measure in noise, and testing protocols for complete robustness. When using S-Series oscilloscopes, engineers benefit from an easy-to-use interface with auto wizards, the best suite of signal integrity test applications, and excellent hardware for signal integrity and deep memory. Newark offers benefits beyond ease-of-use, with same day shipping, access to free online resources and technical support.
“For many engineers, the oscilloscope is the most useful and versatile tool on the bench, so it’s vital that these scopes meet precise test and measurement needs,” said James McGregor, Global Head of Test & Tools, Newark. “Newark is proud to continue offering the latest, most advanced technology from market leaders such as Keysight. This new series of oscilloscopes extends Newark’s already broad offering, and the world class S-Series enables designers and engineers to measure with confidence.”
Keysight is driven to deliver breakthrough solutions and trusted insight in electronic design, test, manufacture, and optimization to help engineers accelerate the innovations that connect and secure the world. Keysight offers unprecedented performance backed by decades of research and expertise.
Newark has increased its on-hand inventory of Keysight products by 15% in the last 12 months and offers discounts on all Keysight products to educational institutions, enabling them to attract new students and support existing ones, even when budgets are tight.
To view the full line of Keysight Infiniium S-Series Oscilloscopes, visit Newark.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/