Full range of ams OSRAM’s OSLON® UV-C LEDs now available from Farnell
ams OSRAM’s OSLON® UV-C LEDs are suitable for a range of disinfection and purification applications.
![FAR584 Inline Image FAR584 Inline Image](https://content.presspage.com/uploads/1564/1920_far584inlineimage.png?10000)
Farnell, an Avnet Company and global distributor of electronic components, products and solutions, is now stocking the full range of ams OSRAM’s OSLON® UV 3636 UV-C LEDs available for fast delivery. Design engineers can access a greater range of market leading UV-C LEDs solutions from ams OSRAM to support a range of purification and disinfection applications such as point-of-use water treatment, automotive interior disinfection, air purification, general disinfection of high touch surfaces, medical environments, home goods and other consumer applications. UV-C LEDs are proven to effectively inactive the SARS-CoV-2 virus.
The OSLON® UV 3636 LED product range emits UV-C radiation and is available in three different power ratings of 4.7mW, 13.5mW, 42mW, enabling designers to select the LED best suited to their application. Each UV-C LED is compact, flexible and harnesses the cleaning properties of UV-C light allowing innovators to make the world cleaner, greener and healthier at the flick of switch. Featuring a robust design, the OSLON® UV-C LED family combines both low and mid-power with a reliable and efficient radiation output.
ams OSRAM’s OSLON® UV 3636 LED product range, now available for fast delivery from Farnell, includes:
• The SU CULCN1.VC provides radiant flux typically of 13.5mW and a radiant efficiency of 2.4 percent.
• The SU CULBN1.VC provides a typical radiant flux output of 4.7mW and radiant efficiency of 2.6 per cent.
• The SU CULDN1.VC is the most powerful in the range providing radiant flux of typically 42 mW and radiant efficiency of 2.1 percent.
Lee Turner, Global Head of Semiconductors and SBC at Farnell said: “Farnell is pleased to offer our customers an extended range of the latest new-to-market UV-C LEDs from ams OSRAM for their designs. ams OSRAM has a long-established reputation for manufacturing innovative optical solutions, offering the highest standards in quality and reliability. Our customers rely on having access to high-quality UV-C components to keep pace with this fast-growing market. The range of optical solutions from ams OSRAM enables our customers to improve quality of life in terms of health, safety and convenience, while reducing impact on the environment.”
The ams OSRAM Group, including the listed companies ams AG as parent company and OSRAM Licht AG, is a global leader in optical solutions. With over 110 years of combined history, ams Osram’s core is defined by imagination, deep engineering expertise and the ability to provide global industrial capacity in sensor and light technologies. By adding intelligence to light, the company enables customers in the consumer, automotive, healthcare and industrial sectors to maintain competitive edge and drive innovation. ams OSRAM works to create technology for breakthrough applications, which is reflected in more than 15,000 granted and applied for patents.
Farnell offers an extensive range of products in its comprehensive semiconductor portfolio to support design engineers. Customers also have free access to online resources, datasheets, application notes, videos, webinars and 24/5 technical support.
Customers can now buy the full range of ams OSRAM’s OSLON® UV 3636 UV-C LEDs with fast delivery from Farnell in EMEA, element14 in APAC and Newark in North America.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/