Farnell signs new distribution agreement with IGS
Intelligent Group Solutions (IGS) offers a wide range of LED modules which can be used as stand-alone products or easily integrated into OEM applications which require visible white, coloured, infra-red or ultraviolet light.
![FAR653 Inline Image FAR653 Inline Image](https://content.presspage.com/uploads/1564/1920_far653inlineimage.png?10000)
Farnell, an Avnet Company and global distributor of electronic components, products and solutions, has signed a new distribution agreement with Intelligent Group Solutions (IGS) to enhance its range of specialist LED lighting solutions. Farnell customers can now access the latest optoelectronic products and LED lighting components offering visible white and coloured light, infra-red and ultraviolet (UV) light from Intelligent LED Solutions (ILS), a division of IGS.
ILS is a leading manufacturer of LED modules which can be used as stand-alone products, or to enable engineers to quickly design-in the latest LED technology into end-products. The vast majority of LED modules feature an aluminium substrate for optimal thermal management and may be used in a wide variety of applications. The range of ILS products now available from Farnell include:
- OSLON® UV 3636 1 LEDiL Selector Board allows design engineers working with the OSLON® UV 3636 LED from OSRAM Opto Semiconductors to easily select associated products when developing lighting systems. This selector board has been designed to work with various silicone optics from LEDiL. It features push-in connectors for ease of use and has predrilled heatsink mounting holes. A compact and powerful light source, the OSLON® UV 3636 LED was designed for equipment illumination, UV-C air disinfection, UV-C surface disinfection, UV-C water disinfection as well as smoke, dust and particle sensing applications.
- PowerStar OSLON® Square contains one of the world’s most compact 2W high power LEDs with extremely low thermal resistance, high efficiency, reliability, and corrosion resistance. The latest generation of the PowerStar OSLON® Square has a 120-degree viewing angle, but it offers enhanced performance and an improved radiation pattern due to an increase in the size of the silicon lens. It is suitable for general lighting, spot lighting, task lighting, decorative lighting, retail and entertainment lighting applications.
- OSLON® Black 4 PowerStar IR is ideal for design engineers working with infrared light and offers all the advantages of the PowerStar range from ILS. Featuring four IR LEDs, the module is suitable for applications requiring high power IR illumination in a compact space, such as surveillance systems, infrared illumination for cameras, machine vision applications, night vision light and driver assistance systems. OSLON® Black Series LEDs from OSRAM Opto Semiconductors are today’s smallest infrared LEDs providing more than 1 watt of optical power.
Lee Turner, Global Head of Semiconductors and SBC at Farnell, said: “We are very pleased to announce our new partnership with IGS and the expansion of our portfolio to include the latest innovations in LED technology from ILS. ILS is quick to market with new LED solutions that integrate cutting-edge products from some of the world’s most trusted global manufacturers. The ILS product range can be easily incorporated into our customers’ products or be used to support design activity of the featured LED. Many ILS products feature Osram LEDs, which are already very popular with our existing customers. Farnell also stocks a wide range of associated products making it easy for customers to find all the components they need to complete their projects with ease.”
Richard Williams, Managing Director of IGS said: “It is fantastic to be working with Farnell. The portfolio we have added into their range is complementary to the products that Farnell offers in the photonics and optoelectronics arena. We look forward to adding many more lines over the coming months and years.”
ILS is one of four divisions of IGS, a specialist company focusing on providing unique solutions to customers requiring optoelectronic components, sub-assemblies and finished products. ILS was formed in response to demand from customers and suppliers requiring specialist products and services in the fast-growing LED sector.
Farnell offers an extensive range of products in its comprehensive semiconductor portfolio to support design engineers. Customers also have free access to online resources, datasheets, application notes, videos, webinars and 24/5 technical support.
The range of LED modules from ILS is now available from Farnell in EMEA and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/