Farnell now stocking fast charging solutions for EVs from Murata
Design engineers can maximise the performance of charging systems with Murata’s market leading solutions for electric vehicle (EV) infrastructure optimisation.
![FAR776 Inline Image - Farnell FAR776 Inline Image - Farnell](https://content.presspage.com/uploads/1564/1920_far776inlineimage-farnell.png?10000)
Farnell, an Avnet Company and global distributor of electronic components, products and solutions, is now shipping fast charging solutions for electric vehicles (EVs) from Murata from stock.
Murata is a global leader in EV infrastructure optimisation, specialising in reliable and durable products designed for the development of leading-edge charging systems.
The enhanced product range from Murata extends Farnell’s comprehensive portfolio of components designed for the development and production of e-mobility systems, including:
· DLW Series Common Mode Choke Coils (CMCC) for Signal and Power line: Design engineers can reduce the common mode noise that is problematic in differential transmission for automotive and EV charging applications using the DLW Series CMCC. It features a low-profile construction and ultra-high self-resonance frequency, enabling high cut-off frequency for high-speed differential lines for Signal line. The DLW Series for power line also offers a large current (6A maximum) suitable for an input connector from an AC adaptor and is available in multiple sizes.
· The MGJ1 Series of DC-DC Converters: An ideal solution for powering ‘high side’ and ‘low side’ gate drive circuits for IGBTs and SIC FETS in inverters. Featuring ultra-low isolation capacitance, continuous barrier withstand voltage 3kVDC, characterised CMTI >200kV/µS and characterised partial discharge performance, the MGJ1 series supports a choice of asymmetric output voltages allows optimum drive levels for best system efficiency. The MGJ1 is also suitable for Medical and factory automation applications.
· DK1 Series Y1 Capacitors: Suitable for all AC-DC switching power supplies where a low-profile is required and lead type capacitors are too large. The DK1 uses a structure of plate-shaped terminals on a disc-shaped ceramic dielectric placed within a plastic mould to reduce the terminal resulting in a mounted height of 2.5mm or less for the product. These safety certified capacitors are placed at the side of a power line input to eliminate noise that builds up primarily in commercial AC power lines. The DK1 series capacitors may also be used in compact AV equipment, LED illumination and 1U rack mounted equipment.
Simon Meadmore, Vice President of Product and Supplier Management at Farnell said: “We are very pleased to be able offer our customers a wide range of fast charging solutions for electric vehicles from Murata. Farnell customers will benefit from Murata’s wide product portfolio, in-stock availability, and other added-value services, such as our dedicated online application guides which are designed to help engineers accelerate time-to-market and maximise the performance of their applications.”
Murata is a leader in the design, manufacture and sale of ceramic-based passive electronic components and solutions, communication modules and power supply modules. The company is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. Murata range of EV charging and power solutions, connectivity modules, sensors and passive components are used in the mobility, communications equipment, healthcare, industrial and personal electronics markets.
Murata’s innovative products for EV fast charging applications are available for delivery from stock at Farnell in EMEA and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/