Leeds,
14
July
2021
|
01:05
Europe/Amsterdam

Farnell now stocking 3D printers from BCN3D Technologies

Customers can now achieve high quality production-grade 3D printing with BCN3D’s unique dual extrusion architecture and independent two-head design.

FAR708_inline

Farnell, an Avnet company and global distributor of electronic components, products and solutions, has added BCN3D Technologies (BCN3D) to enhance its global portfolio of 3D printing products. BCN3D’s range of one-of-a-kind 3D printers are engineered to deliver maximum productivity with hassle-free printing features including large volume production capabilities, full connectivity, and multi-language functions.

BCN3D’s unique dual extrusion architecture with an independent two-head design enables production-grade printing and the delivery of strong functional parts suitable for use in professional, education and industrial sectors. The BCN3D range prints with quality and precision using standard materials including PLA, PET-G, TPU 98A and PVA. All printers feature a range of printing functions including single mode, duplication mode, mirror mode, multi-material mode and soluble supports mode with industrial power for daily operation.

BCN3D’s top-selling range of 3D printers now available from Farnell include:

  • Epsilon W50 and W27 printers are powerful professional 3D printing solutions designed to deliver large-scale parts with industrial grade materials thanks to features such as a passive heated chamber, full enclosure, and humidity controlled environment. The Epsilon W50 and W27 offer improved print quality which is critical when printing in ABS as it is susceptible to warping. The 5" full colour, capacitive touchscreen ensures ease of use and control. Printing is available via Wi-Fi or Ethernet connectivity (online) and an SD Card (offline).
  • Sigma D25 printer is a smaller and lower cost model for Fused Filament Fabrication (FFF). A new generation of BCN3D’s most well-known 3D printer, the Sigma D25 is powered by the Independent Dual Extruder (IDEX) system and quickly delivers functional prototypes with quality and precision.

BCN3D printers have a standard two-year warranty and are open source, allowing customers to use third party materials including the popular 2.85mm Multicomp Pro range available from Farnell.

James McGregor, Global Head of Test, Tools & Production Supplies at Farnell, said: “Farnell continues to partner with the world’s leading innovators in product development and manufacturing to ensure cutting edge technology is available to our global customer base. 3D printing is becoming extremely important in the research and development and industry, and BCN3D are right at the forefront of developing new, innovative solutions to overcome challenges associated with 3D printing. We are pleased that Farnell can offer this exciting and innovative product range to our customers worldwide with fast shipping.”

BCN3D is one of the world’s leading developers and manufacturers of desktop 3D printing solutions, based in Barcelona, Spain. Suitable for professionals and industry level users, BCN3D’s products are designed to be robust, efficient, versatile and adaptable.

Farnell offers a full range of market-leading test, tools and production supplies from stock to support electronic design and test, with no minimum order value and an educational discount programme. Customers have free access to online resources, data sheets, applications notes, videos and webinars with excellent customer and technical support available 24/5 in local language.

BCN3D’s range of cutting-edge 3D Printers are available for fast delivery from Farnell in EMEA, element14 in APAC and Newark in North America.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com

Download Media Kit
Download