Farnell now shipping Nexperia Power GaN FETS for reduced power loss in EVs, 5G and IoT
![FAR603_inline FAR603_inline](https://content.presspage.com/uploads/1564/1920_far603-inline.png?10000)
Farnell, today announced availability of Nexperia’s new to market, innovative Power Gallium Nitride (GaN) FET range. GaN FET products deliver improved density and efficient power usage in a small form factor, enabling the development of efficient systems at a lower cost, and providing the potential to transform power performance in electric vehicles, 5G communications, IoT and more. This innovative range provides real solutions to design engineers as increased legislation, and the growing need to reduce Co2 emissions, drive a shift to more efficient power conversion and increased electrification.
GaN technology overcomes many of the limitations of existing technologies, such as silicon based IGBTs and SiC, to deliver direct and indirect performance benefits to a whole range of power conversion applications. Within electric vehicles, GaN technology directly reduces power losses that can impact the range of a vehicle. More efficient power conversion also reduces the need for cooling systems to dissipate generated heat, reducing the vehicle’s weight and system complexity, in turn leading to a longer operating range or the same range with a smaller battery. Power GaN FETs are also well positioned for applications in data centers, telecom infrastructures, and industrial applications.
GaN FETs deliver superior performance in solutions such as hard switching for AC-DC Totem pole PFC applications, LLC phase shift full-bridge (resonant or fixed frequency) for soft-switching applications, All DC-AC inverter topologies and AC-AC matrix converters using bidirectional switches.
Key benefits include:
› Easy gate drive, low RDS(on), fast switching
› Excellent body diode (Low Vf), low Qrr
› High ruggedness
› Low dynamic RDS(on)
› Stable switching
› Rugged gate bounce immunity (Vth ~ 4 V)
Lee Turner, Global Head of Semiconductors and SBC, Farnell said: “Nexperia is renowned for its extensive portfolio of innovative semiconductor products and we are pleased to further support our customers with the addition of the power GaN FETs to the Farnell range. GaN technology is at the cutting edge of efficient power design and these new products will be a key component to innovative IoT, automotive and communication designs of the future.”
To support customers seeking to adopt GaN FET technology, Farnell and the element14 community hosted a webinar with a Ilian Bonov, GaN International Product Marketing Engineer, from Nexperia, to provide a ‘deep dive’ into this new technology. “Designing High-Efficiency and Robust Industrial Power Supplies with Nexperia GaN FETs”. The webinar overviews the features of Nexperia cascode technology, benefits in hard and soft switching topologies and includes a 4kW Totem Pole PFC Case Study. To find out more about this webinar and watch on demand visit https://www.element14.com/community/events/5572/l/designing-high-efficiency-and-robust-industrial-power-supplies-with-nexperia-gan-fets
The Nexperia Gan FET range is available from Farnell in EMEA, Newark in North America and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/