Bengaluru,
16
January
2025
|
09:49
Europe/Amsterdam

element14 expands line card with the new microBRICK regulator from Vishay Intertechnology

far1110inline

element14 has announced that it is now stocking the band new microBRICK® regulator module from Vishay Intertechnology, expanding its power portfolio with the smallest DC/DC regulator module on the market.

micoBRICK is a synchronous buck regulator module with integrated power MOSFETs and an inductor. It can supply 20 A of continuous current at up to 2 MHz switching frequency.

The regulator produces an adjustable output voltage down to 0.6 V from 4.5 V to 18 V input rail to accommodate a variety computing, consumer electronics, telecom, and industrial applications.

The device’s architecture supports ultrafast transient response with minimum output capacitance, and tight ripple regulation at a very light load. The device is internally compensated and doesn’t require an external ESR network for loop stability purposes.

The device also incorporates a power saving scheme that significantly increases light-load efficiency. The regulator integrates a full protection feature set, including output over voltage protection (OVP), cycle by cycle over current protection (OCP), short circuit protection

(SCP), and thermal shutdown (OTP). It also has UVLO and a user programmable soft start.

The microBrick is available in a lead (Pb)-free power enhanced PowerPAK® MLP60-A6C package measuring only 10.6 mm x 6.5 mm x 3 mm.

Rob Burton, Global Product Segment Leader, Power Management, at element14, said, "Developers need to know what they can achieve with Vishay’s new regulator. As the smallest regulator available on the market today, it has the dual benefits of providing high performance within a small, space-saving footprint.”

Tony Callow, Distribution Account Manager, UK & Eire, for Vishay, added, “microBrick is a simple but effective solution to building efficient high-density DC/DC converters, with a wide input voltage range for a huge range of applications. We look forward to growing our market for these devices with the help of element14’s stocking, ordering, and distribution expertise.”

Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components, which are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH).

Vishay’s new microBrick can be ordered online from Farnell in EMEA, element14 in APAC and Newark in North America.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com/